Technical FAQs

Ask a Question

If the LCD User Interface in SRCE6KUXI model is hanged and not able to change any setting or see any text?

If the LCD User Interface in SRCE6KUXI model is hanged and not able to change any setting or see any text, then wait untill the back-light of LCD goes off (Approximately 2 minutes).
Press any button after the back light goes off. Now see LCD, if the same problem persists kindly contact the customer care.

Note: During this period do not press any button. 
Was this helpful?
What can we do to improve the information ?