Technical FAQs

Ask a Question

If the LCD display is showing fault as Low Battery Shutdown Warning in SRCE6KUXI model?

· UPS is turned on and battery voltage drops below 176v. The alert will appear at the  end of battery discharge.
· The battery cables might be loosely connected to the battery terminals.
· The battery connection to UPS might be loose
Was this helpful?
What can we do to improve the information ?