Technical FAQs

Ask a Question

If the LCD display is showing fault as low run time in SRCE6KUXI model?

. The alert is to warn customer on low state of charge of the battery.
· The alert may appear during On-Line state as well, when estimated state of the charge of the battery is low
· Charge the batteries and look for back-up
· Wait till one charge/discharge cycle is over.
· Please perform the run time calibration test.
· If the Alert persist get the battery health checked.
Was this helpful?
What can we do to improve the information ?