Technical FAQs

Ask a Question

Can I use Gmail or Hotmail email service provider to send email from Magelis HMI programmed by Vijeo Designer.

Vijeo Designer uses only basic SMTP. It currently does not support SSL and other authentication protocols that are used by Gmail and other mail servers. Thus Magelis HMI's are unable to connect to SMTP server of these email services.

It can only connect to SMTP server which do not require any authentication protocols like SSL, TLS etc.
Was this helpful?
What can we do to improve the information ?