Technical FAQs

Ask a Question

Does ClearSCADA support IEC 103 protocol.

The Clear SCADA IEC 60870-5 driver support the following IEC 60870-5 communication protocol.

1. IEC60870-5-101
2. IEC60870-5-104

It do not support IEC103 protocol.
Was this helpful?
What can we do to improve the information ?