Technical FAQs

Ask a Question

What information i get in Unity Pro relating to plc Rack Power supply modules.

Unity Pro software displays the available load and the consumption of all configured power supply modules. Power supply availability is displayed as a bar graph. Each time you add a module, the green bar increases. An overload condition turns the display red. The first time you overshoot the mark, a message is displayed. Nevertheless, you can analyze and generate.
If there is no power supply, the software displays the power consumption requirement in red.
In the case of redundant power supplies, where the full load is applied to each power supply module, the software displays the power supply budget as if there is only one power supply. For summable power supplies, the load is distributed between the power supplies. 
Was this helpful?
What can we do to improve the information ?