Technical FAQs

Ask a Question

Once I add devices to the project after device discovery, what are the actions I need to do before connecting to the device

Once the devices are added after device discovery, you can directly connect to the devices as the communication architecture is made automatically by Ecoreach. 
However, you need to manually create the electrical architecture as per your switchboard electrical architecture. 
Was this helpful?
What can we do to improve the information ?