Technical FAQs

Ask a Question

What is the difference between communication & PC communication in Communication view

Communication section allows entering the communication parameters specifically for Gateway and Serial Interface access points and for the selected device.
When a device is selected from the Tree View, the PC communication section shows the communication interfaces (Local & Network) available for the connection with Ecoreach. 
Was this helpful?
What can we do to improve the information ?