Technical FAQs

Ask a Question

While migrate application program from XBTP021110 to HMI STO using Switch2Vijeo verion 3.40 to convert his existing application of XBTL1000 v4.51 to Vijeo Designer application, but we are getting error with this conversion process.

HMI targets XBTP are not supported by Switch2Vijeo. You can only convert XBTF/FC application.
You will find all supported conversions in the attached help file (Limitations and Conversion >> Conversion >> Converted Terminals).
Was this helpful?
What can we do to improve the information ?