Technical FAQs

Ask a Question

​What is an Ecoreach project & why should I create a project

Ecoreach project includes all devices, modules & communication elements in switchboards which can be further grouped under buildings, floors, zone etc. 
Ecoreach helps you to manage the project lifecycle from Panel Building phase, commissioning phase and then to Maintenance phase. Ecoreach manages the project with the installation description, device hierarchy with localization of switchboards in the building, grouping of devices to the communication access points and helps in project document management as well.
Was this helpful?
What can we do to improve the information ?