Technical FAQs

Ask a Question

How is Ecoreach different from the legacy utility tools

Legacy software tools like RSU & RCU are dedicated to single device settings and focused on commissioning and device diagnostics. Ecoreach software makes the multiple device settings easier and follows the project in different phases by ensuring the user expectations as following.

Ecoreach automatically discovers your smart devices and let multiple devices connected for easy configuration of smart panels. With Ecoreach, you can generate comprehensive reports as part of Factory Acceptance Test and Site Acceptance Test to replace your heavy manual work. Once the panels are under operation, any change of settings made can be easily identified, and hence maintain a system consistency during the operation and maintenance phase.
Was this helpful?
What can we do to improve the information ?