Technical FAQs

Ask a Question

When the CLI (current Limit) function is active on ATV71 drive.

The CLI function is active as soon as the product is running (no stop command).
 The display of CLI can come from:--
- The drive reaches the current limitation (CLI)
- The drive does not follow the acceleration ramp
Was this helpful?
What can we do to improve the information ?