Technical FAQs

Ask a Question

Is it possible to save reference on ATV312 drive when using "+/- speed" function.

Yes, it is possible.
Associated with the "+/- speed" function, this parameter can be used to save the reference:
• When the run commands disappear (saved to RAM)
• When the line supply or the run commands disappear (saved to EEPROM)
Program Parameter Str [Reference saved] => [No] No saving
                                                              => [RAM: Saving in RAM
                                                              => [EEprom] : Saving in EEPROM
Was this helpful?
What can we do to improve the information ?