Technical FAQs

Ask a Question

The XP Style navigation menu is working correctly in my Vijeo Citect project on the server. However in my webclient, the navigation menu is not correctly updating. How can I solve this problem.

The XP Style navigation menu configuration is store in a file menu.dbf in the project folder. For the navigation menu to work correctly in the webclient, this file will need to be deployed to the webclient. The way to do this is to include the menu.dbf file into the within the project folder. 
The problem is that every time you reconfigure the menu, the menu.dbf in the project folder is updated but not the file within the You will need to ensure that the file within the is updated. Follow the below steps to redeploy the project to the webclient. 

1/ Update the within the project folder with the new menu.dbf.

2/ Prepare the project for web deployment.

3/ Login to the webclient as administrator, then edit deployment and then save changes to redeploy the project.

 Also try deleted the Citect folder in %tmp% on the web client bto replicate the changes. 

Make sure that "Fast Runtime Display" is not ticked in the options of the graphics builder the web clients pages will not reflect the changes made in the project and tick "Fast Runtime Display" in the graphics builder before preparing your deployment and updating the changes on the web server. 
Was this helpful?
What can we do to improve the information ?