Technical FAQs

Ask a Question

How to swtich the UPS to Bypass mode from Online mode manually in UPS SRC5KUXI ?

• Bypass mode can be selected through the Control menu screen on the PowerView display

Use the ENTER key to navigate to a main menu and to select user configurable commands.
Go to CONTROL > UPS into Bypass > Confirm Yes 

NOTE :During bypass operation the utility power is connected to the load, bypassing the internal converters. If bypass mode
becomes unavailable the UPS will automatically switch to mains power. In the event that mains power is unavailable
the system will switch to battery power.
Was this helpful?
What can we do to improve the information ?