Technical FAQs

Ask a Question

What are the control power input requirements in PowerLogic PM8000 series meter.

120 to 300 V DC ± 10%
50/60 Hz ± 10% : 90 to 415 V ± 10%400 Hz: 90 to 120 V ± 10%
Was this helpful?
What can we do to improve the information ?