Technical FAQs

Ask a Question

​What is the rating of the current inputs for PowerLogic PM8000 series meter.

Nominal 5 A (Class 0.2S) or 1 A (Class 0.5S)
Measured current: 50 mA to 10 A
Starting current: 5 mA
Withstand: 20 A continuous, 50 A @10 sec/hr, 500 @ 1 sec/hr
Impedance: 0.3 mΩ
Burden: 0.024 VA at 10 A
Was this helpful?
What can we do to improve the information ?