Technical FAQs

Ask a Question

​What are the measurement voltage inputs rated at for PowerLogic PM8000 series meter.

Measured voltage: 57 to 400 V L-N / 100 to 690 V L-L (Wye) or 100 to 600 V L-L (Delta or Wye with unearthed neutral)
Frequency: 50/60 Hz ± 15%,
400 Hz ± 10%
Overload: 600 V L-N or
1035 V L-L
Was this helpful?
What can we do to improve the information ?