Technical FAQs

Ask a Question

What is the default IP address, username, and password for PowerLogic PM8000 series meter.

The default IP address is 

The username and password are defined by your meter’s security configuration; if standard security is enabled, the password is the same as the display password with a default username of 8000. The default display password is 0.
Was this helpful?
What can we do to improve the information ?