Technical FAQs

Ask a Question

With Clear SCADA 2014 we are not able to run its web client over internet using data card for internet connection while web client was running by typing localhost as well as by typing Local LAN IP .

There must be static IP available for the internet connection so that any webX client can connect to the Clear Scada Server. With a data card you always get different IP address on internet for the Clear Scada Server everytime when you connect this data card and for webx clients it would not be possible to connect with SCADA Server.
Was this helpful?
What can we do to improve the information ?