Technical FAQs

Ask a Question

Is it possible to integrate the Modbus Plus protocol in Momentum Unity Plateform.

Yes , modbus plus communication and integration with Momentum unity system can be achieved by the use of Modbus Plus Proxy TCSEGDB23F24FA module.

The Modbus Plus Proxy TCSEGDB23F24FA can be used with Momentum/unity for:
● Modbus Plus Peer Cop
● Modbus Plus Global Data
● 5 byte Modbus Plus message routing
● Unity programming from Modbus Plus to Unity M1E or M1EGD
● Single or dual cable Modbus Plus connectivity
Was this helpful?
What can we do to improve the information ?