Technical FAQs

Ask a Question

What is the maximum output rating for SRC5KUXI / SRC6KUXI ?

The maximum output rating for SRC5KUXI / SRC6KUXI is 220-240 V, 50-60 Hz
Was this helpful?
What can we do to improve the information ?