Technical FAQs

Ask a Question

What are the parameter need to be check while Selecting Fiber Optic Cable for BMXNRP0200 Module.

Parameters are specified by the cable manufacturer and are based on:
  • The wavelength of the optical signal: 1310 nm in the Quantum EIO optical link
  • the cable index: use graded-index cable only
  • the fiber size:
  • 50/125 μm or 62.5/125 μm
  • 9/125 μm
For most multimode optical cable links, the use of 62.5/125 μm cable is recommended because of its relatively low loss and signal distortion.
  • Select the fiber optic cable that meets the demands of your application. Multiconductor cables are recommended.
Most 62.5/125 μm cables are rated at 1.5 dB loss per km. With a multiconductor cable, pairs come with an attenuation specification as measured, which is less than 3.5 dB/km.
Was this helpful?
What can we do to improve the information ?