Technical FAQs

Ask a Question

How we can link external document in Unity pro software.

User can use the hyperlink function available in the Unity Pro software to create links between the project and external documents.
Hyperlinks are shortcuts to such documents as:
  • Installation and wiring diagrams,
  • Help screens,
  • Miscellaneous notes,
  • Images,
  • web pages,
  • etc.
To Add Hyperlink follow the below Steps:
  • Select the Sub-directory under project browser in which Hyperlink to be added.
  • Right click , then select “Add Hyperlink”
  • One popup will be displayed which prompt for the User name and Target path of the file to be opened through that hyperlink.
  • Once above steps have been completed, named link icon will come under the selected directory.
  • Double click on the hyperlink icon to open the attached file.
Was this helpful?
What can we do to improve the information ?