Technical FAQs

Ask a Question

What is the Maximum Number of Entries that can be Possible in LogFile for SoMachine and how it will be handled in case of exceeding the entry.

In SoMachine Max Numbed of Entries for Log File is 65536.
 

After the number is Entry Exceed from Max Numbed of Entries, either it Roll over the previously logged entry or a new entry generates a Log Error. It depends on the Mode selected in LogFile configuration. Circular mode gived the possibility to roll over previously logged entry. No new log file can be created.

 

 
Was this helpful?
What can we do to improve the information ?