Technical FAQs

Ask a Question

How many Vijeo Citect Servers Process can be possible in one Cluster.

In one Cluster of Vijeo Citect there can be following number of Vijeo Citect Server Process can be possible.

1. One Redundant Pair of Alarm Server. (Primary Alarm Server and Standby Alarm Server)
2. One Redundant Pair of Report Server. (Primary Report Server and Standby Report Server)
3. One Redundant Pair of Trend Server. (Primary Trend Server and Standby Trend Server)
4. Unlimited number of IOServer in a Single Cluster.

If you wish to have more than that you need to setup a multiclustered project.
Was this helpful?
What can we do to improve the information ?