Technical FAQs

Ask a Question

In Modicon M221, does it come with the necessary accessories (connector, cable etc) for connecting Built-In Analog Input, or customer requires additional accessories to connect to these two AI channels.

Connector for Built-In Analog Input along with equipped cable is supplied with Modicon M221 controller. It is a dedicated connector and cannot be prepared by user.

In case customer require additional cable connector he can order seperately by ordering the part number TMACBL1.
Was this helpful?
What can we do to improve the information ?