Technical FAQs

Ask a Question

While exporting huge data from Clear Scada using the ODBC query on Excel or MS Access, we encountered "Query time out" error, how can we change this query timeout in Clear SCADA.

To remove this timeout error, you need to chnage the SQL Query parameters in Clear SCADA as shown below :
  • Query Row limit
  • Query Size Limit 
You need to change the default values to your requrements. Also find the attached help file for more details on these parameters.

Was this helpful?
What can we do to improve the information ?