Technical FAQs

Ask a Question

Using HMISCU8B5 can I communicate TM3XTYS4 module to HMISCU8B5

You can not be able to communicate TM3XTYS4 module with HMI SCU as this TM3XTYS4 is a TM3 expansion module which can be connected to TM3 expansion bus only, while with this HMI SCU you can only be able to communicate with CANOPEN supported expansion module.
Was this helpful?
What can we do to improve the information ?