Technical FAQs

Ask a Question

We try to open a page in Vijeo Citect Graphics Builder but not opening, but it opens in Vijeo Citect runtime. How to correct this problem.

Such problems moslty occurs if there is some problem with one of the database file pgdynobj.dbf or pgtouch.dbf, it`s size has become grow much larger. 

The main reason for this error is that in Vijeo Citect SCADA, every graphics object that gets added to a graphics page, gets added to the Pgdynobj.DBF database when the page is saved. However when you remove the object, the line of entry for that particular object in pgdynobj.dbf or pgtouch.dbf sometimes do not get removed. Over time you may get a built up of the pgdynobj.dbf or pgtouch.dbf to a very large size. 

In order to reduce the size you can copy the pgdynobj.dbf or pgtouch.dbf file from your C:\CitectSCADA\User\System or C:\Documents and Settings\All Users\Application Data\Citect\CitectSCADA\User folder over the top of your offending pgtouch.dbf file to zero out the file. 

After copying files from the system folder, complie your project backup and then this problem will resolved.
Was this helpful?
What can we do to improve the information ?