Technical FAQs

Ask a Question

What is tSA in relay assignment on ATV61 drive.

In Monitoring Menu, there is a parameter [Motor thermal state] (tHr).
 
 (tSA) [Th.mot. att.]=> Motor thermal state reached
The THR gives the thermal state of the Motor and ttd is the threshold value for the THR
Example: If you program ttd [Motor therm. level] => 90% and R1[R1 Assignment] => tSA,
Then if [Motor thermal state] (tHr) in Monitoring Menu is reached 90% then Relay will change their state.
Was this helpful?
What can we do to improve the information ?