Technical FAQs

Ask a Question

Is it possible to connect 110V DC input to power supply ABL8REM24030.

There is no difference on performance with the DC input of Power supply ABL8REM24030.
But, when you use DC voltage at the input of ABL8REM24030 power supply, the cULus 508,cCSAus and TUV 60950-1 certifications become invalid.
Was this helpful?
What can we do to improve the information ?