Technical FAQs

Ask a Question

Is it possible to use cycle forward reverse with preset speed adjustable timer with the ATV32 drive.

Yes, it is possible to use cycle forward reverse with preset speed adjustable timer with the ATV32.
Please refer to Note and program example in attachment.
Was this helpful?
What can we do to improve the information ?