Technical FAQs

Ask a Question

Can we use BMXEHC0800 counting module with BMXPRA0100.

No Expert channels (counting, PTO, MPS, NOM, etc.) are supported with BMXPRA0100 refer attached file "General Characteristics of the BMX PRA 0100.PNG". Hence it is not possible to install BMXEHC0800 counting module with BMXPRA0100.

The possible solution is to use other CPU catalog which supports Expert channels as mentioned in attached file "BMX P34 xxxxx Processors Catalog.PNG"
Was this helpful?
What can we do to improve the information ?