Technical FAQs

Ask a Question

Can panel and panel objects get automatically re-sized according to the panel resolution when we change the HMI Target Type in Vijeo Designer having different resolution.

When you change a target's type, model, or resolution (for iPC Smart BOX), the Target Model Change dialog box opens prompting you to verify the change request. 
To automatically scale panel objects in your project to fit into the new screen dimensions, select Automatically resize Panel Contents, Popup Windows, and Font Resources check box and click OK. 

This feature works on Base Panels, Master Panels, Popup Windows, fonts, and font resources.  

"The Automatically resize Panel Contents, Popup Windows, and Font Resources check box  is grayed out, if you change your target to one with same or smaller screen size or resolution."

The automatic resize feautre only works when moving up in screen size. We do not currently support scaling when reducing screen size which is in your case. Also there is no other tool available which can automatically do this. You will have to manually rearrange the the object and its size on the panel.
Was this helpful?
What can we do to improve the information ?