Technical FAQs

Ask a Question

What is the material and plating used for the solder pin of LP4K12015BW3.

On TeSys K range contactor the pin material to make the K contactor ( L*K**5** ) compatible with printed circuit board is made with CuZn15 Cu coated then Tin plated.
Was this helpful?
What can we do to improve the information ?