Technical FAQs

Ask a Question

What is the cross section of the PE cable to connect to the side of the chassis of Masterpact NW.

The cross section of the PE cable to connect to the side of the chassis (there is one hole per side on NW chassis), is 10mm² cable.
Was this helpful?
What can we do to improve the information ?