Technical FAQs

Ask a Question

How can I communicate LTMR100EFM (motor controller LTMR TeSys T) with HMI GTO Series.

Both these devices  LTMR100EFM and HMI GTO having Modbus TCP communication port for which you need to simply use straight LAN cable .
In this HMI GTO you need to create a New Driver using the MODBUS TCP/IP >> Modbus Equipment using which you can communicate with this LTMR100EFM device.
Was this helpful?
What can we do to improve the information ?