Technical FAQs

Ask a Question

Is it possible to switch 24 VAC load through relay outputs of TM221M16R

Yes, it is possible to switch load of 24VAC through relay outputs of TM221M16R

For Resistive load maximum 48 VA that allows switching of 2A current at 24 VAC with guaranteed 100000 nos. of operations.
For inductive load maximum 12 VA that allows switching of 0.5A current at 24 VAC with guaranteed 100000 nos. of operations.
Was this helpful?
What can we do to improve the information ?