Technical FAQs

Ask a Question

What is the maximum numbers of variables can be monitored with M251 webserver.

With M251 webserver, Monitoring Tab: Data parameters sub menu.
The Data Parameters page allows you to create and monitor some lists of variables. User can create several lists of variables (maximum 10 lists), each one containing several variables of the
controller application (maximum 20 variables per list)
So 200 nos. of maximum variables can be monitored on webserver.
Was this helpful?
What can we do to improve the information ?