Technical FAQs

Ask a Question

How to gain access to M241 controller for which password is lost for user enabled access rights

The only way to gain access to M241 controller that has user access-rights enabled and for which user do not have the password(s) is by performing an Update Firmware operation.

This clearing of User Rights can only be accomplished by using a SD card or USB key (depending on the support of your particular controller) to update the controller firmware.

In addition, user may clear the User Rights in the controller by running a script.
This effectively removes the existing application from the controller memory, but restores the ability to access the controller.
 
Was this helpful?
What can we do to improve the information ?