Technical FAQs

Ask a Question

Is TWDPTO220DT - 2 channel PTO module comaptible with M200 controller

TWDPTO220DT - 2 channel PTO module is not compatible to use with M200 controller.

Reasons:
- M200 controller can manage only upto 2 nos. of PTO channels
- TWDPTO220DT is compatible with Twido base and / or M218 base controller only
 
Was this helpful?
What can we do to improve the information ?