Technical FAQs

Ask a Question

Does wireless and battery less pushbutton (XB5R range) have possibility to send a signal when it is dropped to the floor

The working of the transmitter's embedded power supply is based on the principle of the dynamo : the mechanical energy resulting from the moving of a magnet is converted into electrical energy using the electromagnetic induction.
The kinetic energy resulting either from a shock or a rapid deceleration (could be because of dropping down to floor) may cause the moving of the magnet and, consequently, produce enough electrical energy to power the printed circuit board assembly.

So, user has to take it into account for his application while selecting wireless & battery less pushbutton. 
Note : The product is not dedicated for safety application.
Was this helpful?
What can we do to improve the information ?