Technical FAQs

Ask a Question

Which material is used for heat sink in SMPS ABL1REM24062

There are 3 heat sinks used in ABL1REM24062 and the material information are as below : 

HS1(COPPER) : CU1100 
HS2(ALUMINUM) : AL1100 
HS3(ALUMINUM) : AL1100 
Was this helpful?
What can we do to improve the information ?