Technical FAQs

Ask a Question

Can we use Modbus Plus Gateway TCSEGDB23F24FA with Vijeo Citect SCADA to communicate with some devices on modbus plus communication.


You can use Vijeo Citect SCADA to communicate devices on modbus plus using TCSEGDB23F24FA with PLC on MB Plus communication. With Modbus Plus communication as the maximum slave limit that this TCSEGDB23F24FA supports is 127 Numbers. 

Here you have to use MBX driver in Vijeo Citect SCADA to communicate with this Modbus Plus Gateway .
Was this helpful?
What can we do to improve the information ?