Technical FAQs

Ask a Question

Which material is used in the manufacturing of the XB7 Pushbuttons.

XB7 pushbuttons are made of plastic material Polyamide PA
Was this helpful?
What can we do to improve the information ?