Technical FAQs

Ask a Question

Can we add number of clients (View/WebX) with the Clear SCADA Server. Is there is any limitation in term of number of Client add in a system ?

You can add (View/WebX) client license with the CS server and there is a limitation in term of number of Client add in a single license which is 256 number.
Was this helpful?
What can we do to improve the information ?