Technical FAQs

Ask a Question

What is the magnetic tripping threshold for Acti9 DPNa circuit breaker.

The magnetic tripping threshold for Acti9 DPNa circuit breaker is giving below

Magnetic tripping

-> B curve Between 3 and 5 In
-> C curve Between 5 and 10 In
Was this helpful?
What can we do to improve the information ?