Technical FAQs

Ask a Question

What measurements types (that is, "energy", "power", voltage") does the Horizontal Bar gadget support in PME8.0.

The Horizontal Bar gadget support only "Energy" type measurement in PME8.0.
Was this helpful?
What can we do to improve the information ?