Technical FAQs

Ask a Question

What is the degree of protection of Acti9 DPNa circuit breakers.

The degree of protection of Acti9 DPNa circuit breakers is given below:

Degree of protection (IEC 60529)
-> Device only - IP20
-> Device in modular enclosure - IP40 , Insulation class II
Was this helpful?
What can we do to improve the information ?